Hi
I want to using UART to program the EVK. But unable to connect to UART for programming.
Here if the Job I already finish.
1. I Programming the flashloader example into the EVK over Jlink.
2. I able to connection the EVK over USB port and programming it over KinetisFlashTool.
3. I can programming the FW to the start address as 0xa000 over USB port.
4. I trying connect to the EVK over openSDA port with UART mode and I also can get the COMPORT device form the laptop. But When I try to connect it over serial port it will always show :
Error: Connect device failed(Error: Initial ping failure: No response received for ping command.).
The purpose for me is I want to programming the FW over UART.
PS:
I check the UART port configuration of the SDK example and EVK schematic is set the openSDA SDK port as PTB16 and PTB17.
Thanks
Kent Yeh
Hi Kent Yeh,
Please download the frdmk66f_freedom_bootloader to FRDM-K66F board. Then you should be able to connect the FRDM-K66F with it's UART(OpenSDA J26)
The frdmk66f_freedom_bootloader can be found under this folder: \SDK_2_10_0_FRDM-K66F\boards\frdmk66f\bootloader_examples
Best Regards,
Robin
Hi, Robin
Thanks for response. I tried with the example code both for SDK 2.9.0 and 2.10. both of them is not available for me. Does there have any JMP I need to changed
Here is the parameter what I used:
SDK
EVK and connection:
Thanks
Kent Yeh
Please update DAPLink bootloader and firmware (0244_K20DX_FRDMK66F_0X8000.BIN
) of the OpenSDA on FRDM-K66F.
Check if serial port of OpenSDA can communicate properly, for example by running a UART routine.
Hi , Robin
I tried stop the service and programming the 0244_K20DX_FRDMK66F_0X8000.BIN into the address of 0x0000000 and 0x0008000
But still failure. with device connection:
Could you give me your test Firmware, I can verified is it hardware issue
Thanks
Kent Yeh
You can direct drop 0244_K20DX_FRDMK66F_0X8000.BIN (firmware application of K20 on FRDM board) into driver of FRDM. I just want to ensure the serial port of OpenSDA(K20) is working well.
After download the frdmk66f_freedom_bootloader to FRDM-K66F board, you should able to connect it by using KinetisFlashTool.
Hi, Robin
I've update the 0244_k20dx_bl_0x8000.bin file base on the stage of SDA update .
but it's look like malfunction after update it. I can not power the module after connect the SDA port,
Could you tell me how I can repair it
Thanks
Kent Yeh
Hi ,Robin
Now it can not be power on when I connect the SDA USB to my lap.
Therefore. nothing will happen after I press the reset button.
I also try to give module power over USB port. it can be power on but also without any response on the first stage ( Holding the reset button then connect to my lap top).
Kent Yeh