config tool can't be used if the project is created by the chip not in the demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

config tool can't be used if the project is created by the chip not in the demo board

Jump to solution
2,764 Views
Lurkersoo
Contributor III

I use MCUXpresso V11.5, and I’ve installed the related SDK. I create a new project based on LPC55S04, I found its config tool can’t be used. MIt shows that “Device Configuration tool does not support selected processor”. And there are no this kind of problem if the project is based on LPC55S06. Can you help to check what’s wrong with it?

 

0 Kudos
1 Solution
2,749 Views
liborukropec
NXP Employee
NXP Employee

Hi @Lurkersoo ,

for me the latest SDK LPC55S04 2.11 didn't work until I fixed the YAML part in clock_config.c and pin_mux.c - changing LPC55S06 => LPC55S04 otherwise the created Config Tools configuration was empty. If you face the same problem, delete the created *.mex file, fix the sources and open config tools again.

liborukropec_1-1642512932922.png

 

@ZhangJennie , could you please check the YAML parts for the LPC55S04 SDK?

 

Regards,

Libor

View solution in original post

10 Replies
2,732 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI all

Maybe my MCUXpresso IDE version is old. I use v11.3.0. SDK is the latest SDK LPC55S04 2.11.

YAML SETTINGS in clock_config.c and pin_mux.c is LPC55S06

I can open config tool from IDE without issue. 

ZhangJennie_0-1642567595758.png

Thanks,

Jun Zhang

 

0 Kudos
2,724 Views
Lurkersoo
Contributor III

Hi Jun,

We also can open the config tool. You need to try to add a pin configuration, thus you would find the issue. Thanks!

Lurkersoo

0 Kudos
2,720 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Do you mean route a pin in pin configuration ? This is what I see. 

ZhangJennie_1-1642575765962.png

I can't see the error as mentioned in the original request.

 

 

 

 

0 Kudos
2,715 Views
Lurkersoo
Contributor III

Yes, it seems it's ok in you side. 

Lurkersoo

0 Kudos
2,750 Views
liborukropec
NXP Employee
NXP Employee

Hi @Lurkersoo ,

for me the latest SDK LPC55S04 2.11 didn't work until I fixed the YAML part in clock_config.c and pin_mux.c - changing LPC55S06 => LPC55S04 otherwise the created Config Tools configuration was empty. If you face the same problem, delete the created *.mex file, fix the sources and open config tools again.

liborukropec_1-1642512932922.png

 

@ZhangJennie , could you please check the YAML parts for the LPC55S04 SDK?

 

Regards,

Libor

2,579 Views
whiteliondd6
Contributor I

I am using KE16Z64VLD4 and facing the same issue. I make the necessary changes as you suggested changed the MCU in clock_config.c and peripheral.c files. Still, I am not able to use pin config tool and giving me the error: 

The settings do not match for all tools: Boards do not match: Clock 'FRDM_KE16Z' differs from peripherals 'FRDM_KE15Z'

Open configuration failed due to unknown reason

0 Kudos
2,574 Views
ErichStyger
Senior Contributor V

Hi @whiteliondd6 ,

I suggest you make the necessary changes here:

ErichStyger_0-1645684111432.png

 

Erich

0 Kudos
2,569 Views
whiteliondd6
Contributor I

I already applied this step still, facing the error mentioned above

0 Kudos
2,737 Views
Lurkersoo
Contributor III

Hi Libor,

Yes, it seems that we have the same problem. Follow your instruction, it can work now. Thanks a lot!

@ZhangJennie It should be YAML SETTINGS issue, please help to check it. thanks!

0 Kudos
2,752 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Lurkersoo 

Thank you for contacting us.

Did you install the latest LPC55S04 to MCUXpresso IDE?

ZhangJennie_0-1642511118944.png

 

If you use the same SDK version but still have problem, please send your problem screenshot. I will check.

Have a nice day,

Jun Zhang

 

0 Kudos