USB Communication from MIMXRT1170(Host) board to LPC55S28(Device)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Communication from MIMXRT1170(Host) board to LPC55S28(Device)

103 Views
Niranjan123
Contributor I

Hi,

I need to do board to board USB communication from mimxrt1170 evkb board(usb_host_cdc_example) to lpc55s28 board(usb_device_cdc_example) where if I press the reset switch from mimxrt1170 board the led should toogle(blink) in lpc55s28 board, So can you provide any examples related to above same.

thanks,  
Niranjan

0 Kudos
Reply
1 Reply

76 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Niranjan123,

The SDK (version 2.16.1) does not offer an example related this functionality, but in the table 25.3.5 called "Global System Reset Sources" in the RM, are shown the reset sources that you can use for identifying a reset, I hope that could be helpful.
Also, if you experience any issue, do not hesitate to let me know.
BR
Habib.

0 Kudos
Reply