RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX

ソリューションへジャンプ
1,297件の閲覧回数
variable_andrew
Senior Contributor I

Our board has an RT1052 connected to a QSPI Flash W25Q512JV (so larger than default, and QSPI, not HyperFLASH) part.

What is the expected way to connect MCUXpresso to our board with the PEmicro Multilink Unversal FX?

If I use the LPC-Link2 instead, I can just select the RT1052-QSPI generic loader, and it seems to work fine.
But if I want to load FLASH via the Multilink FX - seems I need to do a few more things?

See screenshot:

MCUXpresso w PEmicro

0 件の賞賛
1 解決策
1,282件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @variable_andrew ,

No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.

jingpan_0-1653386684249.png

 

 

Regards,

Jing

 

元の投稿で解決策を見る

2 返答(返信)
1,283件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @variable_andrew ,

No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.

jingpan_0-1653386684249.png

 

 

Regards,

Jing

 

1,296件の閲覧回数
variable_andrew
Senior Contributor I

every time i try to launch with ^^^ - the console only provides the following output:

P&E Semihosting Console

Connection closed by the GDB server.

0 件の賞賛