MCUxpresso IDE SDK K60 FreeRTOS UART example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUxpresso IDE SDK K60 FreeRTOS UART example

951 Views
mschmid
Contributor I

I was able to get the FreeRTOS example for the UART to build but I don't see any UART activity on my console (using  Termite set for 115.2, 8, n,1  PC. UART is working I tested it with a loop back on pins 2 and 3)  the K60 does seem to be running but I can't see any Rx or Tx activity. 

 

I forgot to include my  project files. this may help 

0 Kudos
3 Replies

928 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me with the version of SDK you are using as well as with the IDE you are using ? Is it a custom board or are you using an EVK ?

 

Regards

0 Kudos

924 Views
mschmid
Contributor I

I'm using the TWR-K60D100m evaluation board dated 2012.  

The MCUxpresso IDE is v11.6.0 build 8187, 2022-07-13

I used the on-line tools to create the SDK with the IDE welcome window  'Download and install SDKs' option.

 

Thanks

Michael

0 Kudos

895 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @mschmid,

Could you please confirm your debug console in configuration is in 'UART' instead of 'Semihost' when importing the example?
I apologize, I'm having a hard time trying to understand the problem. Could you please confirm your UART works in loopback, and if so, does it show in the console?

If it does, and the problem is present otherwise, are you using an external device to communicate with the board?

Best regards, Julian

0 Kudos