MCUXpresso IDE doesn't keep the pin configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE doesn't keep the pin configuration

ソリューションへジャンプ
1,516件の閲覧回数
chobin
Contributor III

Dear all,

I'm developing a project for microcontroller K20 using MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05].

I did the pin configuration using Pins section and I saved it.

I have this problem: when I close and open the project, the MCUXpresso doesn't load the pin configuratin and I have to repeat it evrey time.

Does someone know how can I configure the MCUXpresso to load the pin configuration?

Many thanks in advance for your support.

Kind Regards

0 件の賞賛
1 解決策
1,452件の閲覧回数
chobin
Contributor III

Hello,

I solved the problem. There were two *.mix files in the workspace.

Thank you to all.

Kind Regards,

Stefano

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,453件の閲覧回数
chobin
Contributor III

Hello,

I solved the problem. There were two *.mix files in the workspace.

Thank you to all.

Kind Regards,

Stefano

0 件の賞賛
1,452件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Thank you for your input.

Have a nice day!

Regards

Soledad

0 件の賞賛
1,452件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi,

Pins tool configuration is loaded automatically. Be careful if you have several projects in the workspace - Pins tool can open just one configuration. If you modify Pins configuration, hit [Update Code] button to save configuration and apply changes into source code.

Regards

Marek

Regards,
Marek
0 件の賞賛
1,452件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

by Pins section you mean Pins tool probably. Is <projectname>.mex file created in the project? Is there just one *.mex file inside? Would be good if you can attach the mex here.

BTW - are you aware that there's IDE 11.1.0?

Regards,

Libor

0 件の賞賛