Hi @all
I'm using MIMXRT1020 EVK Board , i have imported flexio uart interrupt example from sdk.
I'm able to transmit and receive data at 115200 or even at 500K Baud Rate but if go higher
Baud rate like 1M or 2M not able to get proper data(something like garbage ) but datasheet says it support upto 4M.
please help me out to resolve this issue.
Thanks
#rt1020,#uart#interrupt,#flexiouart
解決済! 解決策の投稿を見る。
Hello, I apologize for the late response, I opened and reviewed the example then I did a compare but I might have an outdated version of the code, could you get the last update and check if the issue is still there, please?
My environment is, IDE: MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17], SDK: 2.14.0
Best regards,
Pavel
@Pavel_Hernandez I have attached code in that i change baud rate and ECHO_BUFFER_LENGTH , nothing more than that.
Thanks
Hello, I apologize for the late response, I opened and reviewed the example then I did a compare but I might have an outdated version of the code, could you get the last update and check if the issue is still there, please?
My environment is, IDE: MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17], SDK: 2.14.0
Best regards,
Pavel
Hello, my name is Pavel, and I will be supporting your case, I have questions about, starting from the example, what modifications you made to the configuration on UART?
Best regards,
Pavel