MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery)

No ratings

MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery)

This tip will show you how to re-trigger a full probe discovery.  The feature is very useful for the customer who may use multiple debug probes.

The first time you debug a project, MCUXpresso IDE will perform a probe discovery operation and display the discovered Debug Probes for selection. This will show all Supported Probes that are attached to your computer. (Here you can see the default P&E Micro OpenSDA of FRDM-KL25Z board was found.)

1 Probe Discovery.png

For any future debug sessions, the stored probe selection will be automatically used to match the project being debugged with the previously used debug probe. This greatly simplifies the case where multiple debug probes are being used.

However, if a debug operation is performed and the previously remembered debug probe cannot be found, then a debug probe discovery operation will be performed from within the same family e.g. MCUXpresso IDE LinkServer, P&E Micro or SEGGER J-Link. (Here you can see there are two Probe search options: Search for PEMicroDBB97E74 again and Search for other attached PE Micro probes.)

But if you want to use a different debug probe(for example: debug FRDM-KL25Z board with SEGGER JLink), click thisdebug_exc.pngblue debug icon will meet problem. Supported Probes dialog only show P&E Micro probes, it will not search other family of debug probes e.g. MCUXpresso IDE LinkServer or SEGGER J-Link.

2 probe not found.png

 

Once a launch configuration file has been created, it will be used for the projects future debug operations. If you wish to use the project with a different debug probe, then simply delete the existing launch configuration and allow a new one to be automatically used on the next debug operation.

3 delet the launch configuration.png

Now click debug_exc.pngblue debug icon re-trigger a full probe discovery, and it show all Supported Probes that are attached to your computer again.

4 new Probe Discovery.png

Labels (1)
Version history
Last update:
‎09-28-2017 08:28 PM
Updated by: