k22 peripheral tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k22 peripheral tool

Jump to solution
956 Views
ulrich_schmidt
Contributor I

Hallo Zusammen,

im MCUXpresso IDE kommt bei der Auswahl des peripheral tools mit dem K22 diese Meldung:

pastedImage_1.png

Welches andere Tool kann ich verwenden und Timer beim K22 zu konfgurieren.

Besten Dank

Ulrich Schmidt

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
857 Views
BlackNight
NXP Employee
NXP Employee

With 'different tool' it means the clocks or the pins tool, as currently the peripherals tool does not support that device (yet).

You can still use the SDK configuration files (without the GUI) to configure the timer.

I would look at the TWR-K21 examples of the SDK, check the FTM timer ones:

pastedImage_1.png

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
1 Reply
858 Views
BlackNight
NXP Employee
NXP Employee

With 'different tool' it means the clocks or the pins tool, as currently the peripherals tool does not support that device (yet).

You can still use the SDK configuration files (without the GUI) to configure the timer.

I would look at the TWR-K21 examples of the SDK, check the FTM timer ones:

pastedImage_1.png

I hope this helps,

Erich

0 Kudos
Reply