Hello NXP, I downloaded the new MCUXpresso IDE v10.1.0. I can build a project but when I click on Flash 'LPCXpresso1769 CMSIS-DAP board’, I get an error message – “No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target”. I have checked the board where the jumper is supposed to go and also I have installed necessary drivers.
Hi Kunal,
What operating system do you work with?
officially we support:
Host operating systems:
Microsoft® Windows® 7/8/10
Ubuntu Linux® (64 bit)
Mac OS X 10.11 and later
Please refer User guide "16.9 Using and troubleshooting LPC-Link2 " for trouble shooting:
https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf
Refer this discussion to update board interface in case on board interface firmware is damaged.
LPC54608 board doesnt see any debug probes
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------