Is it possible to use MCUXpresso with MKL03Z8?An "empty" project almost fills 8K Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use MCUXpresso with MKL03Z8?An "empty" project almost fills 8K Flash

826 Views
diegocolombo
Contributor IV

Hello
I'm very new about MCUXpresso,i spent years with Kinetis Design Studio,and ,working with very small-entry level microcontrollers, I was discouraged to use MCUXpresso anytime I tried.
For example,a new C project,with no semihosting,no peripherals enabled( I mean ,no ADC,no LPTMR..),no rows of code added by me ,Redlib(nohost-nf) occupies 6736 bytes,82,3% of available Flash(and I still need a 1024 bytes sector for saving some data)
If I  select necessary peripherals using SDK Manage Components (ADC,GPIO,PORT,LPTMR,TPM and SPI)
I got  PROGRAM_FLASH: 7532 B 8 KB 91.94%.
I could configure peripherals by hand at register level,but i could find that space will miss, writing my own code.
Is there any way to save some space?

Thanks,
Diego

Tags (1)
0 Kudos
2 Replies

781 Views
ErichStyger
Senior Contributor V

Hi @diegocolombo ,

I suggest you check out an article I wrote on that topic: https://mcuoneclipse.com/2019/08/17/tutorial-how-to-optimize-code-and-ram-size/

It is for a different board/MCU, but the same principles apply. I quickly tried this with the KL03Z, and that way you get easily the code size down to 1.5 kByte. This is kind of the base size without too much limitations, because it includes the necessary clock settings, system and startup code.

That way I even have FreeRTOS running on my KL03Z projects: there is not much legroom on it, but does the job and makes it easy to use.

I hope this helps,

Erich

0 Kudos

790 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello diegocolombo
I replayed your case and if you want to save more space use the -Release build- to optimize your code for better result.

Pavel_Hernandez_2-1645218386142.png

Or I suggest try this option too. Click right in your Project/Properties/C-C++Build/Settings/Tool Settings/Optimization/ and try the different level of optimization.

Pavel_Hernandez_1-1645218367407.png

I suggest use "volatile" for the IRQ.

Regards.

Pavel_Hernandez

0 Kudos