Hello,
HW: RT1170EVK
SW: MCUXpresso v11.5.0
SDK: 2.11.0
when I import an example code from the SDK, I found the XBAR driver library
but how can I create or import this XBAR library by using the MCUXpresso configurator tools? I couldn't find any related XBAR library in the configurator SDK library.
Any someone help?
Solved! Go to Solution.
Hello,
Regarding the routing of the signals via XBARx peripherals – this can be handled via the Pins tool (see picture below). There are used the functions from the fsl_xbara.h or fsl_xbarb.h SDK driver.
Additional note - There is a limitation for signals DMA0 REQ 82~84 signals on i.MX RT117x that there is enabled DMA functionality and set rising edge in the control register for selected request.
However, we are going to create a new Peripherals tool component for handling these signals features (via fsl_xbara SDK driver) with possibility to set interrupt instead of DMA functionality and falling edge of the signal.
Regarding adding of the XBAR driver files to the project - If you want to add fsl_xbara/b drivers to the project, you can use Manage SDK components button (see picture)
Best Regards
Jan Kucera
Hello,
Regarding the routing of the signals via XBARx peripherals – this can be handled via the Pins tool (see picture below). There are used the functions from the fsl_xbara.h or fsl_xbarb.h SDK driver.
Additional note - There is a limitation for signals DMA0 REQ 82~84 signals on i.MX RT117x that there is enabled DMA functionality and set rising edge in the control register for selected request.
However, we are going to create a new Peripherals tool component for handling these signals features (via fsl_xbara SDK driver) with possibility to set interrupt instead of DMA functionality and falling edge of the signal.
Regarding adding of the XBAR driver files to the project - If you want to add fsl_xbara/b drivers to the project, you can use Manage SDK components button (see picture)
Best Regards
Jan Kucera
your suggestion is fantastic. I didn't know the internal signal like XBAR and ADC_ETC_coco can also be configured with PIN configurator.
It is so great - THANKS!!!