On-line live presentations by NXP & related

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On-line live presentations by NXP & related

1,086 Views
dry
Senior Contributor I

I didn't know where to put this question...

I sometimes, see on Linked-In NXP announcements about some on-line tech presentations. Such as, latest I saw something about MCUXPresso coming up, and you could register for the Live one.

Because I'm in very different timezone, I usually can't make them (like, 1 or 2 am start time..).  Do these get recorded, do they get shared other ways? Wouldn't mind to watch recordings too.

Also, can't find them on LinkedIn anymore too.  (Hint where they are?)


Thanks in advance. 

0 Kudos
2 Replies

1,000 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

The mini tech sessions that were recently released can be found on this link:

NXP-EXPERIENCE Mini Tech Sessions

They are all on demand now, so you can watch them at any time. 

Also there are iMXRT Tech Minutes

i.MX RT Tech Minute | NXP 

And in this link you will find general videos, trainings, coming up events:

Training | NXP 

Hope this helps.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos

1,000 Views
dry
Senior Contributor I

Hi Sabina,

Thank you

0 Kudos