BUG REPORT - Typo in MCUXpresso Config Tools generated file for LPADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BUG REPORT - Typo in MCUXpresso Config Tools generated file for LPADC

Jump to solution
1,814 Views
MathiasFriis
Contributor II

Hi there,

I recently ran into an error, where the file peripherals.c autogenerated with the MCUXpresso Config Tools had a typo, when I was trying to configure LPADC1 for a project on 1170-evk.

As seen in the linked image, triggerPriorityPolicy has been misspelled as triggerPrioirtyPolicy in the generated file, which in turn causes a failure to build the project (the "on disk" file is the one I fixed manually).

While it was relatively easy to fix manually, I figured that you would like to know it, so it can be fixed.

 

Best regards,

Mathias

0 Kudos
Reply
1 Solution
1,791 Views
jch
NXP Employee
NXP Employee

Hi Mathias,

there was this typo in the older SDK drivers and we have to have output code the same.

It has been fixed since version 2.2.0 in driver as well as in component version 2.2.0 and newer.

It seems like you have newer driver than component version.

In latest release of Config tools v11, there is menu command for migration to other component version, see attached screenshot.

jch_0-1645032112257.png

 

View solution in original post

1 Reply
1,792 Views
jch
NXP Employee
NXP Employee

Hi Mathias,

there was this typo in the older SDK drivers and we have to have output code the same.

It has been fixed since version 2.2.0 in driver as well as in component version 2.2.0 and newer.

It seems like you have newer driver than component version.

In latest release of Config tools v11, there is menu command for migration to other component version, see attached screenshot.

jch_0-1645032112257.png