mtd-utils for ls1046afrwy repository

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mtd-utils for ls1046afrwy repository

跳至解决方案
380 次查看
williawh
Contributor III

Where should I pull mtd-utils from that is supported by NXP and freescale/layerscape?

I am needing to boot from QSPI with rootfs on NAND IFC similar to:

https://community.nxp.com/t5/Layerscape/Reading-from-a-Ubifs-filesystem-on-LS1046-Freeway/m-p/117877...

https://community.nxp.com/t5/T-Series/T1024RDB-NAND-UIB-ECC-error/m-p/1039573

Need mtd-utils for setting up NAND flash.

Thanks,

William

0 项奖励
1 解答
333 次查看
williawh
Contributor III

I found that if I build the ubuntu:main rootfs, it does contain the mtd-utils...

William

在原帖中查看解决方案

0 项奖励
2 回复数
356 次查看
williawh
Contributor III

Just wondering, once I get the kernel configured properly with mtd, ubi, and ubifs are the necessary commands available at that time or do I still need to install mtd-utils and needed dependencies?

0 项奖励
334 次查看
williawh
Contributor III

I found that if I build the ubuntu:main rootfs, it does contain the mtd-utils...

William

0 项奖励