Use Tamper Detect (TA_TMP_DETECT_B) as GPIO in LS1027A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use Tamper Detect (TA_TMP_DETECT_B) as GPIO in LS1027A

Jump to solution
814 Views
igor_franco
Contributor IV

Hello,

I am working on a customized board with the LS1027AE processor and want to use the Tamper Detect pin as a GPIO to interrupt the processor.

Is this possible? If yes, what are the GPIO group and pin values that represent the Tamper Detect pin?

P.s.: I read in the datasheet that this pin has no additional function. I only want to confirm if it is possible or not.

Best regards,

Igor

0 Kudos
1 Solution
806 Views
ufedor
NXP Employee
NXP Employee

> I read in the datasheet that this pin has no additional function.

This is correct - i.e no way to use the pin/signal as GPIO.

View solution in original post

0 Kudos
2 Replies
800 Views
igor_franco
Contributor IV

Thank you for the fast answer.

0 Kudos
807 Views
ufedor
NXP Employee
NXP Employee

> I read in the datasheet that this pin has no additional function.

This is correct - i.e no way to use the pin/signal as GPIO.

0 Kudos