QorIQ-SDK-V2.0-20160527-yocto.iso image location

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ-SDK-V2.0-20160527-yocto.iso image location

2,326 Views
stevemellor
Contributor I

Where can I find the QorIQ-SDK-V2.0-20160527-yocto.iso image? I have looked on the QorIQ Linux SDK v2.0 Download page and there are a number of ISO files but not with this name. I have downloaded "QorIQ Linux SDK v2.0-1703.tar.bz2" and was trying to follow the installation instructions but failed at the first step.

Thanks.

Steve.

Labels (1)
Tags (1)
0 Kudos
3 Replies

759 Views
srak
Contributor III

Okay. I understand that I need to install 'QorIQ Linux SDK v2.0 SOURCE.iso' to get QorIQ-SDK-V2.0-20160527-yocto

$sudo mkdir /mnt/cdrom
$sudo mount -o loop 'QorIQ Linux SDK v2.0 SOURCE.iso' /mnt/cdrom
$/mnt/cdrom/install

In document, 3.2.2 need to be executed first then do 3.2.1 steps! strange!

0 Kudos

763 Views
srak
Contributor III

I face same problem. I could not find QorIQ-SDK-V2.0-20160527-yocto.iso. I am following the instructions as in 'QorIQ SDK v2.0-1703 Documentation', 

$ tar -xjf SDK-V2.0-1703.tar.bz2
$ ./SDK-V2.0-1703/install

During the install process, the user will be prompted to input the SDK 2.0 ISO installed location, i.e.,
<ISO_INSTALL_PATH>/QorIQ-SDK-V2.0-20160527-yocto.

How to get this QorIQ-SDK-V2.0-20160527-yocto? whether it refers source of SDK here? i.e., 'QorIQ Linux SDK v2.0 SOURCE.iso' ?

0 Kudos

1,545 Views
alexander_yakov
NXP Employee
NXP Employee

There is a number of topics with exact step-by-step instruction on how to install Linux SDK 2.0-1703.

For example, please look this link:

https://community.nxp.com/thread/473019

Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos