PMIC_POR and PORESET

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PMIC_POR and PORESET

跳至解决方案
1,242 次查看
trondwang
Contributor I

Hi NXP,

referring to reset circuit in the schematic of your reference design from Embedded Planet, DES0541_11; page 2:

PMIC_POR_B is connected to R60, but R60 is NOPOP so it will not enter MR_b input of the reset circuit U9.

Instead, PMIC_POR is bypassing the reset circuit through R63 into AND-gate U12 and anded with the RST_ output from U9.

Is there any particular reason why PMIC_POR is bypassing the reset circuit U9?

Could PMIC_POR be connected to MR_b through R60 and instead R63 be NOPOP?

regards Trond Inge 

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,117 次查看
alexander_yakov
NXP Employee
NXP Employee

I do not see a significant difference between PMIC_POR_B connected to U9 and to U12. The difference is only in 140ms duration generated by MIC2774N in response to MR input assertion. As per my understanding, connecting to U9 is not necessary in this case, PMIC itself generates proper timing, so direct connection via AND gate U12 is enough.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,118 次查看
alexander_yakov
NXP Employee
NXP Employee

I do not see a significant difference between PMIC_POR_B connected to U9 and to U12. The difference is only in 140ms duration generated by MIC2774N in response to MR input assertion. As per my understanding, connecting to U9 is not necessary in this case, PMIC itself generates proper timing, so direct connection via AND gate U12 is enough.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------