LS1046A custom board converting cwflash init to PBI commands

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A custom board converting cwflash init to PBI commands

跳至解决方案
997 次查看
JRRandall
Contributor III

Greetings.

we are trying to bring up our custom board based off the LS1046A.  We have had success using cwflash.py and custom scripts based on the LS1046A FRWY init.  The question we have is if there is any automatic or easy way to convert the large number of CCSR address space commands in the DDR4 init script that cwflash uses into PBI commands for running in the BL2/PBL on our target board?

标签 (2)
0 项奖励
1 解答
977 次查看
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.

在原帖中查看解决方案

1 回复
978 次查看
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.