[LS1046A][DPAA][DPDK]fm1-mac9(ethernet@8) can't receive data from dpdk when running l2fwd.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1046A][DPAA][DPDK]fm1-mac9(ethernet@8) can't receive data from dpdk when running l2fwd.

4,174 Views
cecilia_zhong
Contributor I

Hi

I have been running l2fwd with interface fm1-mac5(ethernet@4) and I can receive data from dpdk. I can run l2fwd with interface fm1-mac9(ethernet@8) but I can't receive data from dpdk.

The config data file and the pcd file we used as below.

<classification name="dpdk_mac5_classif" masks="yes">
<key>
<fieldref name ="ipv4.nextp"/>
</key>
<entry>
<vsp name="dpdk_mac5_flows" />
<data>0x11</data>
<mask>0xFF</mask>
<queue base="0x900" count="1"/>
</entry>
<entry>
<vsp name="dpdk_mac5_flows" />
<data>0x32</data>
<mask>0xFF</mask>
<queue base="0x900" count="1"/>
</entry>
<action condition="on-miss" type="distribution" name="default_mac5_dist"/>
</classification>

<distribution name="dpdk_mac5_dist">
<vsp name="dpdk_mac5_flows" />
<protocols>
<protocolref name="ipv4"/>
</protocols>
<queue base="0x900" count="1"/>
<action type="classification" name="dpdk_mac5_classif" />
</distribution>

<distribution name="default_mac5_dist">
<vsp name="shared_mac_pool" />
<queue count="1" base="0x88"/>
</distribution>

<classification name="dpdk_mac9_classif" masks="yes">
<key>
<fieldref name ="ipv4.nextp"/>
</key>
<entry>
<vsp name="dpdk_mac9_flows" />
<data>0x11</data>
<mask>0xFF</mask>
<queue base="0xb00" count="1"/>
</entry>
<entry>
<vsp name="dpdk_mac9_flows" />
<data>0x32</data>
<mask>0xFF</mask>
<queue base="0xb00" count="1"/>
</entry>
<action condition="on-miss" type="distribution" name="default_mac9_dist"/>
</classification>

<distribution name="dpdk_mac9_dist">
<vsp name="dpdk_mac9_flows" />
<protocols>
<protocolref name="ipv4"/>
</protocols>
<queue base="0xb00" count="1"/>
<action type="classification" name="dpdk_mac9_classif" />
</distribution>

<distribution name="default_mac9_dist">
<vsp name="shared_mac_pool" />
<queue count="1" base="0x8a"/>
</distribution>

What can I check to know why the fm1-mac9 can't receive data from dpdk?

Port statistics ====================================
Statistics for port 0 ------------------------------
Packets sent: 0
Packets received: 0
Packets dropped: 0
Aggregate statistics ===============================
Total packets sent: 0
Total packets received: 0
Total packets dropped: 0
====================================================

0 Kudos
Reply
20 Replies

3,959 Views
cecilia_zhong
Contributor I

For the TPM the mac9 and mac10 is used for 10g phy, in our side, we connect the 1g phy the same as the mac5, but mac5 can work, is there some limitation on mac9 with 1G phy for dpdk vsp mode?

 

0 Kudos
Reply

3,954 Views
yipingwang
NXP TechSupport
NXP TechSupport

mac9 with 1G phy cannot work.

0 Kudos
Reply

3,947 Views
cecilia_zhong
Contributor I

what's the meaning of mac9 with 1G phy can't work? dpdk vsp can't work? What's the limitation on it?

0 Kudos
Reply

3,935 Views
yipingwang
NXP TechSupport
NXP TechSupport

If the negotiation between MAC9 and your 1G PHY is successful, then it can work in Linux Kernel, it could also work in the DPDK VSP scenario. VSP has no relation with the link of PHY MAC.

0 Kudos
Reply

3,915 Views
cecilia_zhong
Contributor I

Based on our test, in kernel mode it is working, but vsp is not working with 1G Phy, and from the fman code in lsdk, we checked mac9 and mac10 is hardcode as 10G, does this configuration will casue the vsp not working with 1G phy? How can we debug further?

0 Kudos
Reply

3,908 Views
yipingwang
NXP TechSupport
NXP TechSupport
This is the fix for this issue from DPDK development team: https://github.com/NXPmicro/dpdk/commit/fc5be5f0ac99f34c801152de7f6165cf65cf8ff4
0 Kudos
Reply

3,906 Views
cecilia_zhong
Contributor I
Yes I have updated this code, but the issue can't be fixed. And we found that there are counters with 1a00000.fman/1a90000.port and 1a00000.fman/1ab0000.port, which are fm1-mac9 fman port. But the FQ is empty. -sh-4.4# cat /sys/devices/platform/soc/1a00000.fman/1a90000.port/statistics/* fm0-port-rx6 counter: 0 fm0-port-rx6 counter: 0 fm0-port-rx6 counter: 1042 fm0-port-rx6 counter: 1051 fm0-port-rx6 counter: 0 fm0-port-rx6 counter: 0 fm0-port-rx6 counter: 0 fm0-port-rx6 counter: 9 -sh-4.4# cat /sys/devices/platform/soc/1a00000.fman/1ab0000.port/statistics/* fm0-port-tx6 counter: 1292 fm0-port-tx6 counter: 1295 fm0-port-tx6 counter: 0 fm0-port-tx6 counter: 1301 fm0-port-tx6 counter: 0 fm0-port-tx6 counter: 1307 fm0-port-tx6 counter: 1310 fm0-port-tx6 counter: 0 fm0-port-tx6 counter: 0 -sh-4.4# echo 0xd00 > query_fq_np_fields -sh-4.4# cat query_fq_np_fields Query FQ Non Programmable Fields Result fqid 0xd00 force eligible pending: no retirement pending: no state: Tentatively Scheduled fq_link: 0x0 odp_seq: 0 orp_nesn: 0 orp_ea_hseq: 0 orp_ea_tseq: 0 orp_ea_hptr: 0x0 orp_ea_tptr: 0x0 pfdr_hptr: 0x0 pfdr_tptr: 0x0 is: ics_surp contains a surplus ics_surp: 0 byte_cnt: 0 frm_cnt: 0 ra1_sfdr: 0x800 ra2_sfdr: 0x0 od1_sfdr: 0x0 od2_sfdr: 0x0 od3_sfdr: 0x0 -sh-4.4#
0 Kudos
Reply

3,895 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please run  debug_dump.sh script and send us the output.

This script is typically present in /usr/local/dpdk directory on the board.

Or you can copy it from dpdk/nxp/ source code.

0 Kudos
Reply

3,890 Views
cecilia_zhong
Contributor I

Please find the attach output file dpdk_debug__01011970_000756_mac9.txt for debug_dump.sh script .

0 Kudos
Reply

3,874 Views
yipingwang
NXP TechSupport
NXP TechSupport

   Can you run it with following command as well:

 

/home/l2fwd -w fm1-mac9 -c 0x3 -n 1 --file-prefix=p1 --socket-mem=1024 --log-level=eal,8 --log-level=dpaa,8 -- -p 0x1 -q 1

 

This will give use dpaa bus related logs

0 Kudos
Reply

3,870 Views
cecilia_zhong
Contributor I

Hi

Please find the attached files, thanks.

BR

0 Kudos
Reply

3,951 Views
cecilia_zhong
Contributor I
Can I modify the code to make it work? How can I do?
0 Kudos
Reply

4,042 Views
cecilia_zhong
Contributor I

Hi,

How to defined the queue base="0xb00" in the policy xml?

0 Kudos
Reply

4,034 Views
yipingwang
NXP TechSupport
NXP TechSupport

Did fm1-mac9 work normally when you use the default policy files provided in LSDK 21.08?

0 Kudos
Reply

4,162 Views
yipingwang
NXP TechSupport
NXP TechSupport

Did you use VSP scenario?
Did you boot the target board with dtb file fsl-ls1046a-rdb-usdpaa-shared.dtb?

Please setup VSP fmc configuration as the following to check whether ethernet@8 can receive data from DPDK.

$ fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046_shared_24g.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_24g_classif_udp_ipsec_1queue.xml -a

Did you check whether fm1-mac9 can work in Linux?

0 Kudos
Reply

4,159 Views
cecilia_zhong
Contributor I

Yes, I use the VSP scenario and boot the target board with dtb file fsl-ls1046a-rdb-usdpaa-shared.dtb.

I have setuped VSP fmc configuration as you saided.

I have checked fm1-mac9 can work in Linux(I can setup my device to connect mme and make ue attach, but can not ping the device form mme). So I confirmed I can receive data from kernel, but can not receive data from dpdk.

When I change to fm1-mac5(ethernet@4), I can receive data from dpdk.

BR

0 Kudos
Reply

4,151 Views
yipingwang
NXP TechSupport
NXP TechSupport

Do you have ls1046ardb demo board?

If yes, please run all your configurations on LS1046ARDB to do verification.

0 Kudos
Reply

4,149 Views
cecilia_zhong
Contributor I
Yes, what I used to run the l2fwd is ls1046ardb board.
0 Kudos
Reply

4,050 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please use fsl-ls1046a-rdb-usdpaa-shared.dtb and xml files /usr/local/dpdk/dpaa/usdpaa_config_ls1046_shared_24g.xml and /usr/local/dpdk/dpaa/usdpaa_policy_24g_classif_udp_ipsec_1queue.xm all from LSDK 21.08 default configuration, it seems that you have modified /usr/local/dpdk/dpaa/usdpaa_policy_24g_classif_udp_ipsec_1queue.xml.

0 Kudos
Reply

3,855 Views
cecilia_zhong
Contributor I

Hi NXP,

One thing need highlight here is,in our project we used the mac9 and mac10 connect with 1G phy solution, not 10G phy,I think the reference board is 10G phy based, is there anything we need to change to support 1G phy on mac9 for dpaa vsp feature.

 

0 Kudos
Reply