LS1043A DPAA work queue strict-only scheduling in a channel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043A DPAA work queue strict-only scheduling in a channel

跳至解决方案
845 次查看
cyrilstrejc
Contributor III

In LS1043A DPAA hardware, current work queue (WQ) scheduling follows two level scheduler schema, which is mixture of strict and round-robin prioritization.

wx-prioritization.png

Is somehow possible to simplify the DPAA approach and use only 8 strict priorities with round robin completely disabled? (WQ 0 -> Priority 0, WQ 1 -> Priority 1, WQ 2 -> Priority 2, ..., WQ 7 -> Priority 7. Higher priority WQ has absolute strict priority over all lower priority WQs)

标签 (1)
标记 (1)
0 项奖励
1 解答
715 次查看
alexander_yakov
NXP Employee
NXP Employee

It is not possible to use 8 strict priorities. In other words, it's not possible to disable round robin selection that is used for medium and low priority tiers.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
716 次查看
alexander_yakov
NXP Employee
NXP Employee

It is not possible to use 8 strict priorities. In other words, it's not possible to disable round robin selection that is used for medium and low priority tiers.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------