Hi,
we are producing a test run of open hardware LS1028A SOMs and chip supplies are low. Currently we designed for LS1028AXE7PQA or LS1028ASE7PQA. But LS1028AXN7PQA and LS1028ASN7PQA could also be good options, I just can't figure out from the manuals if the Armv8 crypto extensions are disabled in the N variant (opposed to E) or not. We don't need features such as secure boot, but crypto extensions are important because of performance. Can someone give us a reliable answer?
Best Regards
Lukas
Hi @mntmn,
LS1028AXN7PQA and LS1028ASN7PQA doesn't have crypto extension as crypto hardware is disabled.
Regards,
Mrudang