LS1028 DPDK port status seems to be wrong

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028 DPDK port status seems to be wrong

1,811 Views
Gourmet
Contributor I

My board is LS1028 which has ETH ports for 1000Mbps, I verified it by iperf3.

However, when I tried  DPDK (which 1028 is supported), Something went wrong:

following the document, I first change the dtb with the DPDK one, then run the /dpdk_configure_1028ardb.sh. 

 

I started my DPDK test by:

./dpdk-testpmd -l 0-1 -n 4 -- -i --portmask=0x1 --nb-cores=1

 

logs here:

EAL: Detected CPU lcores: 2
EAL: Detected NUMA nodes: 1
EAL: Detected static linkage of DPDK
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'VA'
EAL: No available 32768 kB hugepages reported
EAL: No available 64 kB hugepages reported
EAL: No available 1048576 kB hugepages reported
EAL: VFIO support initialized
EAL: Using IOMMU type 1 (Type 1)
EAL: Probe PCI driver: net_enetc (1957:e100) device: 0000:00:00.0 (socket 0)
EAL: Probe PCI driver: net_enetc (1957:e100) device: 0000:00:00.6 (socket 0)
enetc_net: MAC is not available for this SI, set random MAC

enetc_net: New address: E6:54:C7:C4:08:B8

TELEMETRY: No legacy callbacks, legacy socket not created
Interactive-mode selected
previous number of forwarding ports 2 - changed to number of configured ports 1
testpmd: create a new mbuf pool <mb_pool_0>: n=155456, size=2176, socket=0
testpmd: preferred mempool ops selected: ring_mp_mc

Warning! port-topology=paired and odd forward ports number, the last port will pair with itself.

Configuring Port 0 (socket 0)
Port 0: 02:D1:30:03:DA:3E
Configuring Port 1 (socket 0)
Port 1: E6:54:C7:C4:08:B8
Checking link statuses...
Done
testpmd>

 

 

then taping : show port info all

 

********************* Infos for port 0  *********************

MAC address: 02:D1:30:03:DA:3E

Device name: 0000:00:00.0

Driver name: net_enetc

Firmware-version: not available

Connect to socket: 0

memory allocation on the socket: 0

Link status: down

Link speed: 10 Mbps

Link duplex: half-duplex

Autoneg status: Off

MTU: 1500

Promiscuous mode: enabled

Allmulticast mode: disabled

Maximum number of MAC addresses: 0

Maximum number of MAC addresses of hash filtering: 0

VLAN offload: 

  strip off, filter off, extend off, qinq strip off

No RSS offload flow type is supported.

Minimum size of RX buffer: 0

Maximum configurable length of RX packet: 9600

Maximum configurable size of LRO aggregated packet: 0

Current number of RX queues: 1

Max possible RX queues: 1

Max possible number of RXDs per queue: 64000

Min possible number of RXDs per queue: 32

RXDs number alignment: 8

Current number of TX queues: 1

Max possible TX queues: 2

Max possible number of TXDs per queue: 64000

Min possible number of TXDs per queue: 32

TXDs number alignment: 8

Max segment number per packet: 0

Max segment number per MTU/TSO: 0

Device capabilities: 0x0( )

 

********************* Infos for port 1  *********************

MAC address: E6:54:C7:C4:08:B8

Device name: 0000:00:00.6

Driver name: net_enetc

Firmware-version: not available

Connect to socket: 0

memory allocation on the socket: 0

Link status: down

Link speed: 10 Mbps

Link duplex: half-duplex

Autoneg status: Off

MTU: 1500

Promiscuous mode: enabled

Allmulticast mode: disabled

Maximum number of MAC addresses: 0

Maximum number of MAC addresses of hash filtering: 0

VLAN offload: 

  strip off, filter off, extend off, qinq strip off

No RSS offload flow type is supported.

Minimum size of RX buffer: 0

Maximum configurable length of RX packet: 9600

Maximum configurable size of LRO aggregated packet: 0

Current number of RX queues: 1

Max possible RX queues: 1

Max possible number of RXDs per queue: 64000

Min possible number of RXDs per queue: 32

RXDs number alignment: 8

Current number of TX queues: 1

Max possible TX queues: 2

Max possible number of TXDs per queue: 64000

Min possible number of TXDs per queue: 32

TXDs number alignment: 8

Max segment number per packet: 0

Max segment number per MTU/TSO: 0

Device capabilities: 0x0( )

testpmd> 

 

(tried with --iova-mode=pa also, but nothing changed)

but my port status should be 1000Mbps with full duplex, what's going on?  Is there anything wrong with my configuration or hardware? 

 

Yours sincerely

A student counting on this to graduate  begging for help

Labels (1)
Tags (1)
0 Kudos
1 Reply

1,798 Views
Gourmet
Contributor I

By reading DPDK source code, 10Mbps and half duplex are the default case as the result of switch registers reading, when the reading result goes wrong, then 10M and half will be the status.

 

0 Kudos