LS1021A-TWR: Full reprogram

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A-TWR: Full reprogram

1,211 次查看
z_v
Contributor I

Hello,

In order to reprogram the original image I did the following:

SW2 - 01001111

SW3 - 01100101

(This is setup I got here)

But in CW I got the message:

Error: The algorithm was not able to run on the target of the flash is not configured properly

Error: Getting flash ID failed

Can you please help ?

Both banks are currently not running.

Thank you,

Z.V

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,099 次查看
z_v
Contributor I

Hello,

I recreated the CW RAM application project.

Now programming works fine.

Thank you !

Z.V

0 项奖励
回复

1,099 次查看
ufedor
NXP Employee
NXP Employee

Which exactly TWR revision is in question?

Please provide photos of the on-board inscriptions and stickers.

Please provide additional information about CodeWarrior setup:

1) which Debug Configuration is used?

2) complete Flash Programmer log as a text file

0 项奖励
回复