How to control GPIO ISR affinity in SDK 2.0 on the LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to control GPIO ISR affinity in SDK 2.0 on the LS1043A

1,708 Views
pro-supportengi
NXP Employee
NXP Employee

1) How do customer's control GPIO ISR affinity in SDK 2.0? At this point we don’t know how to assign these interrupts to any core other than Core#0.

2) It looks like the existing GPIO driver does not support assigning interrupts to any other core than CPU0, is this correct? 

3) If so, why are GPIO interrupts assigned only to Core#0?

4) There are virtual GPIO interrpts and GPIO hardware interrupts, can either or both interrupts be assigned to a specific core other than Core#0?

Creating the GPIO interrupt on 1043:

root@ls1043ardb:~# echo 498 > /sys/class/gpio/export

root@ls1043ardb:~# echo falling > /sys/class/gpio/gpio498/edge

root@ls1043ardb:~# cat /proc/interrupts

             CPU0         CPU1       CPU2       CPU3

[....]        

66:            0            0          0          0     GIC 106

Level        1740000.jr

67:            0            0          0          0     mpc8xxx-gpio   18

Edge         gpiolib

IPI0:          3226         4833       4237      4170   Recheduling interrupts

IPI1:            17           21         19        23   Function call interrupts

Setting GPIO affinity doesn’t work:

root@ls1043ardb:~# echo 1 > /proc/irq/67/smp_affinity_list

-sh: echo: write error: Input/output error

Setting eMMC interrupt affinity works just fine:

root@ls1043ardb:~# echo 1 > /proc/irq/12/smp_affinity_list

root@ls1043ardb:~# cat /proc/interrupts

             CPU0         CPU1       CPU2       CPU3

[....]        

1:            0            0          0          0     GIC 29

Edge        arch_timer

2:           35475          39336    28975       38803 GIC 30

Edge        arch_timer

11             9           0          0           0    GIC 75 Level    fsl-ifc

12:           3370         14         0           0    GIC 94 Level    mmc0

[...]

Labels (1)
0 Kudos
2 Replies

1,144 Views
pro-supportengi
NXP Employee
NXP Employee

Hi Pavel,

following your instructions from the web sites above, the customer tried the following but was unable to set the smp_affinity for IRQ 67 below.  Do you know why? 

root@ls1043ardb:~# cat /proc/irq/67/smp_affinity

f

root@ls1043ardb:~# echo 2 > /proc/irq/67/smp_affinity

-sh: echo: write error: Input/output error

root@ls1043ardb:~# echo f > /proc/irq/67/smp_affinity

-sh: echo: write error: Input/output error

root@ls1043ardb:~# echo 498 > /sys/class/gpio/export

root@ls1043ardb:~# echo falling > /sys/class/gpio/gpio498/edge

root@ls1043ardb:~# cat /proc/interrupts

             CPU0         CPU1       CPU2       CPU3

[....]        

66:            0            0          0          0     GIC 106

Level        1740000.jr

67:            0            0          0          0     mpc8xxx-gpio   18

Edge         gpiolib

IPI0:          3226         4833       4237      4170   Recheduling interrupts

IPI1:            17           21         19        23   Function call interrupts

Also, there are 4 GPIO blocks and 4 interrupts respectively:

98 GPIO1

99 GPIO2

100 GPIO3

166 GPIO4

So it’s expected to see them in /proc/interrupts like other GIC’s interrupts with appropriate numbers (or at least with a single/common to all GPIOs number).

Unable to see the GPIO blocks in /proc/interrupts on SDK 2.0, do you know why? Specifics will be helpful.

0 Kudos

1,144 Views
Pavel
NXP Employee
NXP Employee

Look at the following pages:

https://access.redhat.com/documentation/en-US/Red_Hat_Enterprise_Linux/6/html/Performance_Tuning_Gui...

and

https://cs.uwaterloo.ca/~brecht/servers/apic/SMP-affinity.txt

and

http://www.thegeekstuff.com/2014/01/linux-interrupts/?utm_source=feedburner

See also the following page from NXP Community:

https://community.nxp.com/thread/301130


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos