Code example and DTS configuration for IRQ5 signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code example and DTS configuration for IRQ5 signal

跳至解决方案
869 次查看
lucroy
Contributor III

Currenlty working with the LS1021 and looking for a code example and DTS configuration to trigger an interrupt service routine from IRQ5 signal or any of the six available IRQ signals. 

标签 (1)
0 项奖励
1 解答
748 次查看
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

在原帖中查看解决方案

0 项奖励
2 回复数
749 次查看
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

0 项奖励
748 次查看
Pavel
NXP Employee
NXP Employee

See attached files.

These file are .dts file from LSDK 1906 for the LS1088ARDB board.

Find IRQ10 in the fsl-ls1088a-rdb.dts file.

The LS1088ARDB board uses interrupt from the PCF2129.

 

NXP Linux BSP supports sysfs possibility for GPIO interrupt using. Use this possibility for your application.

 

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励