Can you run Baremetal on the LS2088A ARM cores?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you run Baremetal on the LS2088A ARM cores?

Jump to solution
562 Views
joseph_lindula
Contributor IV

Hello, quick question for the community members. Is it possible to run baremetal programs on the LS2088A, or is it required to run Linux?

Joe

1 Solution
518 Views
ufedor
NXP Employee
NXP Employee

There are no baremetal examples and applications for the LS2088A from NXP.

View solution in original post

2 Replies
519 Views
ufedor
NXP Employee
NXP Employee

There are no baremetal examples and applications for the LS2088A from NXP.

518 Views
joseph_lindula
Contributor IV

Hello, thanks for responding to my post. So, it is possible to write a baremetal application?

0 Kudos