Activate snvs on ls1021atwr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activate snvs on ls1021atwr

734件の閲覧回数
letailleurjerom
Contributor I

hi all,

I work on ls1021atwr with cpld V2.0.

I work in secure world and I would like to use the snvs device.

I have a imx snvs inplémentation but does not work with ls1021atwr.

Do you need to activate a special clock?

Do you have a snvs implémentation guide?

 thanks for you help.

Best Regards.

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

577件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello letailleur jerome,

Please refer to secure boot section from "Submit Form ".

SNVS is security monitor block, you could refer to the section "Security monitor" in LS1021A Reference user manual for details.

Please refer to the following to setup the board for secure boot flow.

a. Flow A
Program the ITS fuse. Use RCW with SB_EN=0
Or
b. Flow B
For prototyping phase, don't blow the ITS fuse, but use rcw with SB_EN = 1.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛