16-bit QSPI chip with LS1046A-based board

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

16-bit QSPI chip with LS1046A-based board

ソリューションへジャンプ
575件の閲覧回数
JRRandall
Contributor III

Hi,

We have a 16-bit QSPI chip we are trying to use as the boot device for our LS1046A-based board.  We noticed in the LS1046A FRWY initialization PBI commands there is a command that looks like it's setting the QuadSPI_MCR to 64-bit LE (write 0x550000, 0x000f400c).

Questions:

Are we able to use 16-bit QuadSPI on with the LS1046A? It looks like all the NXP designs use 8-bit QSPI, which is probably compatible with switching the endianness like this.

Will a 16-bit QSPI be able to endian swap on the qspi controller?

ラベル(1)
0 件の賞賛
1 解決策
570件の閲覧回数
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

元の投稿で解決策を見る

0 件の賞賛
1 返信
571件の閲覧回数
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

0 件の賞賛