Flash layout for new boot flow with TF-A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash layout for new boot flow with TF-A

評価なし

Flash layout for new boot flow with TF-A

Please note that the LSDK memory layout for TF-A boot flow explained in this topic is only applicable for LSDK 18.12 and newer releases. 

The following table shows the memory layout of various firmware stored in NOR/NAND/QSPI flash device or SD card on all QorIQ Reference Design Boards.

When the board boots from NOR flash, the NOR bank from which the board boots is considered as the "current bank" and the other bank is considered as the "alternate bank". For example, if LS1043ARDB boots from NOR bank 4, to update an image on NOR bank 0, you need to use the "alternate bank" address range,0x64000000 - 0x64F00000.
Firmware Definition MaxSize Flash Offset (QSPI/NAND flash) Absolute address (NOR bank 0 on LS1043ARDB, LS1021ATWR)

Absolute address 

(NOR bank 4 LS1043ARDB, LS1021ATWR)

Absolute address (NOR bank 0 on LS2088ARDB)

Absolute address

(NOR bank 4 on LS2088ARDB)

SD Start Block No.
RCW + PBI + BL2 (bl2.pbl) 1 MiB 0x00000000 0x60000000 0x64000000 0x580000000

0x584000000

0x00008
ATF FIP Image (fip.bin) BL31 + BL32 + BL33 4 MiB 0x00100000 0x60100000 0x64100000 0x580100000 0x584100000 0x00800
Boot firmware environment 1 MiB 0x00500000 0x60500000 0x64500000 0x580500000 0x584500000 0x02800
Secure boot headers 2 MiB 0x00600000 0x60600000 0x64600000 0x580600000 0x584600000 0x03000
Secure header or DDR PHY FW 512 KiB 0x00800000 0x60800000 0x64800000 0x580800000 0x584800000 0x04000
Fuse provisioning header 512 KiB 0x00880000 0x60880000 0x64880000 0x580880000 0x584880000 0x04400
DPAA1 FMAN ucode 256 KiB 0x00900000 0x60900000 0x64900000 0x580900000 0x584900000 0x04800
QE/uQE firmware 256 KiB 0x00940000 0x60940000 0x64940000 0x580940000 0x584940000 0x04A00
Ethernet PHY firmware 256 KiB 0x00980000 0x60980000 0x64980000 0x580980000 0x584980000 0x04C00
Script for flashing image 256 KiB 0x009C0000 0x609C0000 0x649C0000 0x5809C0000 0x5849C0000 0x04E00
DPAA2-MC or PFE firmware 3 MiB 0x00A00000 0x60A00000 0x64A00000 0x580A00000 0x584A00000 0x05000
DPAA2 DPL 1 MiB 0x00D00000 0x60D00000 0x64D00000 0x580D00000 0x584D00000 0x06800
DPAA2 DPC 1 MiB 0x00E00000 0x60E00000 0x64E00000 0x580E00000 0x584E00000 0x07000
Device tree(needed by uefi) 1 MiB 0x00F00000 0x60F00000 0x64F00000 0x580F00000 0x584F00000 0x07800
Kernel lsdk_linux.itb 16 MiB 0x01000000 NA NA NA NA 0x08000
Ramdisk rfs 32 MiB 0x02000000 NA NA NA NA 0x10000

The following figures highlight the changes in the flash layout for previous boot flow (with PPA) and flash layout for TF-A boot flow.

Flash layout for previous boot flow (with PPA)

 

PPA-flash-layout.png

Changed flash layout for TF-A boot flow

TFA-flash-layout.png

ラベル(2)
バージョン履歴
最終更新日:
‎09-10-2020 02:56 AM
更新者: