Where is my license file stored?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is my license file stored?

2,437 Views
lpcware-support
Senior Contributor I

After going through the activation process, your LPCXpresso IDE (v6 and later) license files are stored in a directory called "NXPLPCXpresso". This is the same regardless of whether you are using a Free license or a Pro license.

The location of this directory depends on the host operating system, and the directory must be writable by the user running LPCXpresso IDE.

Windows XP

  • The location of the directory is %ALLUSERSPROFILE%, where %ALLUSERSPROFILE% is an environment variable whose value is typically "C:\Documents and Settings\All Users".

Windows Vista / 7 / 8

  • The location of the directory is %PUBLIC%, where %PUBLIC% is an environment variable whose value is typically "C:\Users\Public".

Linux

  • The location of the directory is "/usr/share".

Mac OSX

  • The location of the directory is "/Users/Shared".

Earlier Code Red toolchains

Earlier Code Red toolchains stored the license directory in the same root directory as specified above. However the name of the license directory itself was different. This allows different toolchains to be installed and licensed at the same time.

  • Red Suite 5.x: RedSuite5
  • Red Suite 4.x: RedSuite
  • Red Suite 3.x: red_suite
  • LPCXpresso (v5 and earlier): LPCXpresso
Labels (1)
Tags (2)
0 Kudos
0 Replies