Status bar shortcuts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Status bar shortcuts

940 次查看
lpcware-support
Senior Contributor I

The 'Status Bar', at the bottom of the LPCXpresso IDE, has a useful set of hot links looking something like the image below:

146581_146581.pngstatusbar.png

  • Hover over the project name to reveal the full system path to your project or workspace.

  • Click on the project name or workspace name and a file browser window will open.

  • Control-click on the project name or workspace name and a command prompt (Terminal, Console) window will open.

  • Click on the Processor/Microcontroller Vendor name, and a browser window will open at their site.

  • Click on the Processor/Microcontroller Part Number, and a browser window will open at a page describing the part.

  • Control-click on the Processor/Microcontroller Part Number, and the MCU Settings dialog in Project Properties will open.

Note : You can also open a command prompt or a file browser window from the Utilities entry of the Project Explorer view's context sensitive, right-click, menu.

Submitted on Thu, 2016-03-17 06:15

标签 (1)
标记 (2)
0 项奖励
0 回复数