how to flash LPC54102 board wihtout using lpcexpresso software at the customer end?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to flash LPC54102 board wihtout using lpcexpresso software at the customer end?

1,223 次查看
chethankumar
Contributor III

Hi,

I am using board which contains LPC54102 chip. I want to update the firmware(newly created axf) of the board without using LPCExpresso IDE. What are the possible solutions available (ex:USB, UART or Wi-Fi)? Can it flashed using script?.

Please point us to the relevant document or any pre-written script.

Thanks,

ck

标签 (4)
0 项奖励
回复
2 回复数

947 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

The user manual contains a chapter entitled 'the Flash API' which contains all the information you should need. Alternatively you could look at a tool such as FlashMagic Flash Magic - Welcome . Note you may need to extract the binary from the .axf image.

Yours,

LPCXpresso support

0 项奖励
回复

947 次查看
chethankumar
Contributor III

Hi,

Is it possible to program the LPC54102 using LPCScript as suggested by below link

http://www.nxp.com/files/microcontrollers/doc/user_guide/LPCScrypt_User_Guide.pdf?fasp=1&WT_TYPE=Use...
However above link is for  LPC18/43 family. If it is possible to program the LPC54102 also can you provide the necessary script?.

Thanks,
Ck
0 项奖励
回复