Drop in replacement for OM13056

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Drop in replacement for OM13056

1,454 Views
thomaspeter-volpi
Contributor II

Hi

We are trying to get a hold of a few OM13056 LPCXpresso boards (8 units max.), but none of the big distributors have it in stock.  

Is there maybe a drop-in replacement for the OM13056 available? We have a custom PBC that is plugged onto the header sockets of an OM13056 and we would like to reproduce that setup.

Best regards 

Thomas

 

Labels (1)
Tags (1)
8 Replies

1,390 Views
thomaspeter-volpi
Contributor II

Hi XiangJun 

I tried https://www.nxp.com/part/OM13056#/, but the major distributors don't have it in stock. I also don't need a drop in replacement for the board and its headers, not the chip LPC1549JBD64. If there is another LPCXpresso board with the same header interface that can run the same software as the OM13056 I would be happy with that.

Best regards

Thomas

0 Kudos
Reply

1,383 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you just use Arduino header, it is okay, a lot of board has the Arduino header.

Can you tell us the header signals you are using?

BR

XiangJun Rong

0 Kudos
Reply

1,374 Views
thomaspeter-volpi
Contributor II

Arduino.pngThis is how we use the Arduino header interface.

I suppose the OM13058 would work (https://www.nxp.com/part/OM13058#/), but I don't know how much we would have to change the firmware that was written for the OM13056 to be running on the OM13058. Or would it be pretty straightforward to port a firmware for the OM13056 to the OM13058?

0 Kudos
Reply

1,331 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If the connector signals match between OM13056 and OM13058, porting the firmware is not a huge task, because all the code is written with C language.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

1,369 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The OM13058 is based on LPC11U68, which uses Cortex-M0 core.

If you have the source code and just use GPIO, uart, ADC, I do not think the task is huge.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

1,351 Views
thomaspeter-volpi
Contributor II

Hi

Is there another NXP MCU DevKit with Arduino headers that uses an ARM Cortex-M3 microcontroller?

Best regards

Thomas

0 Kudos
Reply

1,341 Views
frank_m
Senior Contributor III

Other vendors like ST have Arduino-compatible headers as well.
Like most of their Discover and Nucleo boards.
However, I consider their "Cube" library/SDK a regular disaster.

0 Kudos
Reply

1,423 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the OM13056 board, it is also called LPCXpresso1549, which uses LPC1549JBD64 processor.

I suppose that there is not Drop in replacement for LPC1549JBD64 

It appears that you can order the silicon  from the link:

https://www.nxp.com/part/LPC1549JBD64#/

For the OM13056 board ordering, pls try the website:

https://www.nxp.com/part/OM13056#/

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply