Will the KV10 or KV11 be supported in Kinetis SDK v2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will the KV10 or KV11 be supported in Kinetis SDK v2?

ソリューションへジャンプ
833件の閲覧回数
kylemanna
Contributor II

Will the KV10 or KV11 be supported in Kinetis SDK v2?  I see that they are supported in Kinetis SDK v1.3, but I'd like to use v2.0.

 

Thanks!

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
698件の閲覧回数
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
699件の閲覧回数
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

0 件の賞賛
返信
698件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Kyle,

no, only these details in the document are relevant.

No early access is not possible.

Best Regards,

Iva

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信