Difference between SDK_2.0_MK65FN2M0xxx18 and SDK_2.0_TWR-K65F180M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between SDK_2.0_MK65FN2M0xxx18 and SDK_2.0_TWR-K65F180M

706件の閲覧回数
biafra
Senior Contributor I


Hi everyone,

 

At the moment I'm working with tower system TWR-K65F180M, but soon I will work with my own board mounting MK65FN2M0VMI18 device.

For this reason I created two SDK 2.0 with the online SDK builder tool: one for the tower system (SDK_2.0_TWR-K65F180M) and the other for the device I use in my board (SDK_2.0_MK65FN2M0xxx18).

I noticed that the two SDK I created are identical: is there a reason for this or is there a bug in the builder?

 

Many thanks for the answer

Biafra

ラベル(1)
1 返信

404件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Francesco,

Regarding your question, I think the package is the same for the SDK_2.0_MK65FN2M0xxx18 and SDK_2.0_TWR-K65F180M. What the difference is only the memory size, it is okay to change the linker file and modify the memory size, then recompile the project.

Hope it can help you.

BR

Xiangjun Rong