nxpMClib_v1.0_0 library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nxpMClib_v1.0_0 library

542 Views
babaei_pouya
Contributor I

Hi,

i'm using nxpMClib_v1.0_0 library for PMSM motors, but is there any description about that example code?

best regards,

pouya

Tags (1)
0 Kudos
1 Reply

410 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pouya,

You can download the library of motor control from the link:

Real Time Control Embedded Software Motor Control and Power Conversion Libraries|NXP 

After you install the library, you can read the pdf file which describes every function in detail.

C:\Freescale\FSLESL\doc\56800EX_FSLESL_4.2_doc

Regarding the PMSM FOC control basic theory, pls refer to the an1931 from the link:

https://www.nxp.com/docs/en/application-note/AN1931.pdf 

Hope it can help you

BR

Xiangjun Rong

0 Kudos