need product mark of MK02FN64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need product mark of MK02FN64

658 Views
andes
NXP Employee
NXP Employee

I checked the datasheet of "Kinetis K02 64 KB/128 KB Flash, Rev. 3, 4/2015", there is product mark of 32pin/48pin device, but no this infomation for 64pin. please state the product mark of 64pin K02, MPN is MK02FN64VLH10. Thanks.

please feedback to andes.gao@nxp.com

thanks!

Andes

0 Kudos
3 Replies

399 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Yudong,

Why you said there is no 64pin K02 ?

The chip MK02FN64VLH10 is 64 pin。

pastedImage_0.png

You can check the detail information in the K02F Sub-Family Reference Manual .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

399 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Alice

I believe that the customer asking for the body mark, not for the ordering part number

If this is the case, tomorrow I will send you the information

Regards

0 Kudos

399 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi I got it

The marking is the hole part number

"MK02FN64VLH10"

0 Kudos