frdm-kea128 i have this evolution board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

frdm-kea128 i have this evolution board

473 次查看
SBK_SBK_SBK_SBK
Contributor I

frdm-kea128 i have this evolution board. may i program this through code warrior IDE. or it will only supports S32

 

0 项奖励
回复
1 回复

462 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi SUMANA_BHAT_K,

Please download FRDM-KEA Quick start package (REV 8 ) or Sample Software Drivers for KEAZ64/128 using S32DS from FRDM-KEAZ128: KEA Freedom Evaluation Board website.
Those examples are developed with S32 Design Studio for Arm 2018.R1 – Windows/Linux(REV 2018-R1).

Or you can use CodeWarrior 11.x if you are familiar with CodeWarrior+Processor Expert, but there is no official SDK examples.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复