What is "M20AGV 1N86B CTEXGBE" mean by a k20dx128vlf5 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is "M20AGV 1N86B CTEXGBE" mean by a k20dx128vlf5 ?

跳至解决方案
4,329 次查看
rqbh
Contributor III

I have some k20dx128vlf5, but  there is "M20AGV 1N86B CTEXGBE" on the surface of the chip, what is that mean?

or is there some rules to read it means ? thanks

标签 (1)
0 项奖励
1 解答
1,675 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

M20AGV is the way that Freescale has coded the "K20DX128VLF5" part number for devices that are too little to write the whole part number.

1N86B is the silicon mask revision. Each device has several revisions, with the known erratas related to each revision.

CTEXGBE is the data code, it gives information of when and where has been manufactured the chip.

Regards,

Santiago

在原帖中查看解决方案

0 项奖励
2 回复数
1,676 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

M20AGV is the way that Freescale has coded the "K20DX128VLF5" part number for devices that are too little to write the whole part number.

1N86B is the silicon mask revision. Each device has several revisions, with the known erratas related to each revision.

CTEXGBE is the data code, it gives information of when and where has been manufactured the chip.

Regards,

Santiago

0 项奖励
1,675 次查看
rqbh
Contributor III

I see, thanks a lot !

0 项奖励