What is "M20AGV 1N86B CTEXGBE" mean by a k20dx128vlf5 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is "M20AGV 1N86B CTEXGBE" mean by a k20dx128vlf5 ?

ソリューションへジャンプ
4,327件の閲覧回数
rqbh
Contributor III

I have some k20dx128vlf5, but  there is "M20AGV 1N86B CTEXGBE" on the surface of the chip, what is that mean?

or is there some rules to read it means ? thanks

ラベル(1)
0 件の賞賛
1 解決策
1,673件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

M20AGV is the way that Freescale has coded the "K20DX128VLF5" part number for devices that are too little to write the whole part number.

1N86B is the silicon mask revision. Each device has several revisions, with the known erratas related to each revision.

CTEXGBE is the data code, it gives information of when and where has been manufactured the chip.

Regards,

Santiago

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,674件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

M20AGV is the way that Freescale has coded the "K20DX128VLF5" part number for devices that are too little to write the whole part number.

1N86B is the silicon mask revision. Each device has several revisions, with the known erratas related to each revision.

CTEXGBE is the data code, it gives information of when and where has been manufactured the chip.

Regards,

Santiago

0 件の賞賛
1,673件の閲覧回数
rqbh
Contributor III

I see, thanks a lot !

0 件の賞賛