UART DMA and CTS

cancel
Showing results for 
Search instead for 
Did you mean: 

UART DMA and CTS

Jump to solution
472 Views
lsrbigfoot
Contributor III

Does the UART-CTS input signal (when activated) have the ability to block/unblock UART-Tx DMA traffic automatically (without processor intervention)?

If not, then what extra controls are required to make this happen?

Labels (1)
0 Kudos
1 Solution
298 Views
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

View solution in original post

0 Kudos
1 Reply
299 Views
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

0 Kudos