Servomotors control with FRDM-KE02Z

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Servomotors control with FRDM-KE02Z

評価なし

Servomotors control with FRDM-KE02Z

Using five channels from FTM2 module of the KE02 microcontroller included on the FRDM-KE02Z board for controlling a robotic arm powered by five servomotors. Each servomotor is controlled by a couple of buttons of a matrix keyboard, which is connected to eigth GPIOs. Interrupts are not used in this example. The code was generated and compiled on CodeWarrior for Microcontrollers v10.5.

添付
コメント

A video is available at the following link:

https://community.freescale.com/videos/1768

This is great. I have a Robix kit from when i was a kid with the old parallel port interface, this is a great upgrade. Thanks for posting.

バージョン履歴
最終更新日:
‎12-08-2013 02:03 PM
更新者: