MKE02Z: Accuracy of trimmed Internal Oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE02Z: Accuracy of trimmed Internal Oscillator

1,046件の閲覧回数
colin_campbell
Contributor II

Hi NXP,

We are implementing an MKE02Z16VFM4 CPU based design and would like to confirm the accuracy of the trimmed Internal Oscillator as supplied by the Factory.

Our application uses the Internal Reference Clock in FEI Mode with the fixed 1024 Multiplier, to produce a nominal source clock frequency of 32 MHz. Our reading of the Data Sheet (Table 12: Num 9, 11 and 12) and Reference Manual suggests that each MKE02Z16VFM4 device is supplied pre-trimmed by the Factory, thereby allowing the device to meet the IRC accuracy specification of -1/+0.5% over the full temperature range (-40 to +105C), without any further calibration by the end user - is this correct?

Thanks for the guidance - CC

MKE02Z16VFM4 _irc_spec.PNG

ラベル(2)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

841件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

The end customer can trim internal reference clock of ICS by their own. You may would like to make reference this post:

https://community.nxp.com/docs/DOC-95356 

0 件の賞賛
返信

841件の閲覧回数
colin_campbell
Contributor II

Hi NXP,

Thank you for the confirmation that the nominal Internal Oscillator Frequency can be trimmed by the end user - that makes sense.

The key item we wanted to confirm is our understanding that each MKE02Z16VFM4 device is supplied pre-trimmed by the Factory to a nominal Internal Oscillator Frequency of 31.25 kHz, which will have an accuracy specification of -1/+0.5% over the full temperature range (-40 to +105C), without any further calibration by the end user - is this correct?

Thanks for the additional guidance - CC

0 件の賞賛
返信

841件の閲覧回数
miduo
NXP Employee
NXP Employee

Sorry for the late response. Yes, correctly!

0 件の賞賛
返信

841件の閲覧回数
colin_campbell
Contributor II

Hi NXP,

 

Thank you for the confirmation on the accuracy of the trimmed Internal Oscillator as supplied by the Factory - that makes sense.

 

Many thanks - CC

0 件の賞賛
返信