Hello,
I am 2 TWR-K70F120M board
In one sdcard is working ,and other its not working
following is the output for mmc info command
Device: FSL_SDHC
Manufacturer ID: 3
OEM: 5344
Name: SL16G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 15931539456
Bus Width: 1-bit
In the working tower board ,its showing
Bus Width: 4-bit
rest data is same
What might be the issue ,is this problem there with the other k70 tower boards,
How to rectify ?
Hi,
Could you please provide the TWR-K70F120M board hardware version info?
If both boards with the same hardware version?
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Both have same version sch-27166 Rev B1
Hi,
Sorry for the later reply.
I checked the system record, there without related info before.
Please check here to warranty replacement that issued TWR-K70F120M board. Thanks.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------