How to ensure that witch PIT channel is used for SKEAZ64 ?

取消
显示结果 
搜索替代 
您的意思是: 

How to ensure that witch PIT channel is used for SKEAZ64 ?

226 次查看
547416104
Contributor III

Hello EveryOne,

I just used Codewarrior11.0 ProcessorExpert to configure PIT module, I do not know witch PIT channel should be configured, and do not how to ensure witch PIT channel is used by MCU.

My question is how to ensure whitch PIT channel is used by the MCU?

The detail information as the follow picture, thanks!

547416104_0-1656172869339.png

 

0 项奖励
1 回复

213 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

These two articles may help you understand how to use Processor Expert:
Overview: Processor Expert
Getting Help on Processor Expert Components

There are several examples of typical settings and usage of xxx_LDD component. You can modify the setting in processor expert and copy the codes.

_LDD Typical Usage.png

Do you want to use LPIT for timed interrupts? Then you can refer to using TimerInt_LDD.

TimerInt_LDD.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励