Does MKL25Z128VLK4 support flash swap?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MKL25Z128VLK4 support flash swap?

ソリューションへジャンプ
1,561件の閲覧回数
tuowang
Contributor II

Hi everyone,

I have a Kinetis KL25Z evaluation board with MKL25Z128VLK4. Does this MCU support flash swap feature?

Thanks

Tuo

ラベル(2)
タグ(4)
0 件の賞賛
1 解決策
1,321件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tuo Wang:

KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
1,322件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tuo Wang:

KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
1,068件の閲覧回数
gamine99
Contributor I

Hello Jorge,

We are currently using an MK60DN512, but due to its difficulty to source, we are considering using the MK60DN256ZVLL10 and urgently need to know if the flash swap feature is supported in the DN256 as this is critical to our application.

Also, do you know what the "Z" refers to and what Errata may exist for that part (DC 2019+).

Thank you!

0 件の賞賛
1,321件の閲覧回数
tuowang
Contributor II

Thank you, Jorge! That's very helpful. Can you advise if there is any L series MCU that supports flash swap? Thanks Tuo

0 件の賞賛
1,321件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

You are welcome.

Unfortunately none of the L series support flash swap.

Regards!

Jorge Gonzalez

0 件の賞賛
1,321件の閲覧回数
tuowang
Contributor II

Thank you Jorge!

0 件の賞賛