Could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F?

543 Views
gloria
Contributor III

Hi, could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F? If yes, how could I do it? Many thanks!

Labels (1)
0 Kudos
1 Reply

323 Views
mjbcswitzerland
Specialist V

Hi

The FTM (used for PWM) can be optionally clocked from the MCGFFCLK but not directly from OSCERCLK.

See µTasker MCG Configuration Support

Depending on the configuration of the MCG ,MCGFFCLK may be related to OSCERCLK (or derived from it) but it is highly unlikely that it will be the same frequency.

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support  / µTasker Kinetis TWR-K64F120M support  / µTasker Kinetis TWR-K65F180M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos