Cant use PEmicro debugger with KL46Z256M4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cant use PEmicro debugger with KL46Z256M4

524 次查看
denisc7slzo
Contributor I

Dear sirs, 

i got frdm - kl46z, i was working with this board before and had no problems, now when i want to debbug it doesn't work for me and i got errors like this. I need help please. 

Screenshot 2022-11-16 231553.png

Screenshot 2022-11-16 231638.png

Captura de pantalla (10).png

 

OS: WINDOWS 11 
PROGRAM VERSION: MCUXpresso IDE v11.6.1_8255
The board turns on the steady green led normally and the system detects it 

The board turns on the steady green led normally and the system detects it

 

0 项奖励
回复
1 回复

506 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi denisc7slzo,

Please put the attached bin file into the FRDM-KL46Z driver. Does the D5 LED blink red?

If so, please try to debug your project with MCUXpresso IDE v11.6.1_8255.

If D5 LED doesn't blink red. Then you may need to use the Kinetis_Recovery_Utility discussed in "MK60DX256VLL10" RESET PIN


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复