Can't create MCUXpresso Project using MKM34Z256VLL7 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't create MCUXpresso Project using MKM34Z256VLL7 ?

跳至解决方案
509 次查看
GanesanGuru
Contributor IV

Hi team,

I've followed this link, for working with Custom HWs, where the SDK for LPCXpresso845MAX in imported and used to create a new breakout board.During the process, the device package has been modified/changed to suit the application. It worked perfectly for me without any glitches.

Similarly, I imported both SDK_2_14_0_TWR-KM34Z75M & SDK_2_14_0_MKM34Z256xxx7  -- and when i changed the default device package to MKM34Z256VLL7 (where my custom board is gonna be build based on this package), the project build without any error. But, when I go for the config tools- pin modifications in project I'm getting the below error.

Then to create a project for MKM34Z256VLL7? 

 

Screenshot from 2023-10-19 19-06-28.png

标签 (1)
0 项奖励
1 解答
483 次查看
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).

在原帖中查看解决方案

1 回复
484 次查看
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).